Failed to read device signature (operation failed, reading signature)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

 Failed to read device signature (operation failed, reading signature)

7,584 Views
evoluer
Contributor I
Hello all,
I am having a problem for the last 3 weeks and i am not able to find a solution for it. Let me explain the problem in detail.
When i try to download the program, i get the following error Failed to read device signature ( operation failed .(reading signature)). Accessing a device using the wrong protocol could render the device unusable. Do you want to continue?
controller: lpc2148
oscillator: 12MHz crystal
serial connection through max3232
reset and program switch connection
Software used : Flashmagic version9.73.4146 arm7 UART driver version: 5.00.3965
Hope someone can point me in the right direction
Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

3,394 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Nanda,

You could take a look at the following links:

https://www.olimex.com/Products/ARM/NXP/LPC-P2106/resources/How-to-use-LPC-P2106-with-FlashMagic.pdf

http://www.edaboard.com/thread242593.html

http://forum.flashmagictool.com/index.php?topic=3645

 
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply