FDI-LPC3250-Ethernet Diconnecting Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FDI-LPC3250-Ethernet Diconnecting Issue

1,019 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pradeep Kumar on Wed Jan 08 06:30:32 MST 2014
Hi,

I am using LPC-3250 custom board ported with kernel 2.6.34.For file system mounting i'm using ramdiskboot and mtdboot procedures.When the board is getting powered in that time ethernet is connected properly and i'm running applications on board .But after some time in both the booting procedure  ethernet getting disconnected. In H/W side on board ICS1893AFI IC is mounted for ethernet interfacing.

  The following dmesgs are getting when i'm using ramdiskboot procedure

   nfs: server 192.168.1.10 not responding, still trying

How can i recetify this issue on LPC3250.Can any one suggest me to get out of this issue.


Thanks In Adv &  Regards,


Pradeep Kumar G.
Labels (1)
0 Kudos
Reply
0 Replies