External circuitry required for USB0_PWR_FAULT in LPC4367

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External circuitry required for USB0_PWR_FAULT in LPC4367

2,724件の閲覧回数
akhilesh_sreedh
Contributor III

Hello,

The datasheet of LPC4367 provides USB0_PWR_FAULT functionality with the description "Port power fault signal indicating overcurrent condition; this signal monitors over-current on the USB bus (external circuitry required to detect over-current condition)." What exact external circuitry is required, is there any document or application note for the external circuit?  

Thanks

Akhilesh

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,375件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

You can use the LPC4330-Xplorer Board schematic file as reference

pastedImage_1.png


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------