External circuitry required for USB0_PWR_FAULT in LPC4367

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

External circuitry required for USB0_PWR_FAULT in LPC4367

2,746 次查看
akhilesh_sreedh
Contributor III

Hello,

The datasheet of LPC4367 provides USB0_PWR_FAULT functionality with the description "Port power fault signal indicating overcurrent condition; this signal monitors over-current on the USB bus (external circuitry required to detect over-current condition)." What exact external circuitry is required, is there any document or application note for the external circuit?  

Thanks

Akhilesh

标签 (2)
标记 (2)
0 项奖励
回复
1 回复

1,397 次查看
soledad
NXP Employee
NXP Employee

Hi,

You can use the LPC4330-Xplorer Board schematic file as reference

pastedImage_1.png


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------