External Trigger to HSADC using SGPIO10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External Trigger to HSADC using SGPIO10

2,380件の閲覧回数
shivam0078
Contributor I

Kindly suggest a way to trigger HSADC of LPC 4370 using SGPIO10. If possible then please send the snippet of the code as well. @ravithakur 

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

2,372件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

we do not know what logic of SGPIO you would like to implement, anyway, I think an11275.zip is helpful for your understanding SGPIO module, pls refer to it.

Hope it can help you

https://www.nxp.com.cn/docs/en/application-note/AN11275.zip

 

BR

XiangJun Rong

0 件の賞賛
返信

2,305件の閲覧回数
shivam0078
Contributor I

Thanks for your reply. I want a trigger pin using which I can trigger the hsadc externally in lpc link 2 board. From the datasheet I have found that I can trigger the hsadc using SGPIO10. I have configured the sgpio10 to the P1_3 pin of LPC4370 controller. Then I have connected the SGPIO10 as a trigger to HSADC using GIMA. Please suggest me a way to trigger HSADC externally.

 

0 件の賞賛
返信