Export Raw Data

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Export Raw Data

跳至解决方案
19,993 次查看
Skyrise
Contributor II

Hi, 

I'm trying to do some power consumption measures on my LPC55S69 with the MCU Link Pro debugger. I want to export those measures on my computer and display them on octave (same as matlab) but the problem is that the .bin generated with all the data is in a specific format that I can't understand. 

Basically, I understood that there is a header of 22 bytes with for example, the magic number which is 4 bytes long. The problem is that I don't know the type of variable that is coded is it a float, fixed, int, uint? And this is the problem with all the variable in this file. The doc that I have is linked to this post. 

If someone could help me with this it would be nice, 

Thank you.

LOMBARD Loris 

0 项奖励
回复
1 解答
19,514 次查看
ErichStyger
Specialist I

Hi @Skyrise ,

that's really good news!

I did update my article on https://mcuoneclipse.com/2023/07/30/data-converter-for-mcuxpresso-energy-measurement-data/ with the latest findings.

I hope others will benefit from this too.

在原帖中查看解决方案

0 项奖励
回复
16 回复数
19,975 次查看
ErichStyger
Specialist I

Hi @Skyrise ,

I'm working right now on a converter program (work in progress):

ErichStyger_0-1690482870155.png

 

In short: You will need to do some byte swapping. The data items need to be multiplied/divided as in the documentation explained. The 64bit timestamp and average values are IEEE64 encoded, and here again you need to do byte swapping and then multiply/divide.

I have not sorted out the 'log' for the min-avg-max sequence.

0 项奖励
回复
19,923 次查看
Skyrise
Contributor II

Hi, @ErichStyger 

Thanks to your explanations and your screen I managed to "almost" plot my signal. I think the problem is that sometimes I have incorrect values which is due to this number of summary values that I don't manage to understand at which frequency they are in the binary file...

I linked to this message my signal which is between 0.03 and 0.035 and as you can see there is a lot of incorrect values which are due to those summary values. 

 

0 项奖励
回复
19,919 次查看
ErichStyger
Specialist I

I'm struggling with the same issue as you (frequency of summary records). I need to read the data in the context of a university research project I'm doing with an external partner. Give me some time to clean-up the source code, so I can make it available?

0 项奖励
回复
19,915 次查看
Skyrise
Contributor II

Did you find the source code of the debug plot for the power measurement in MCUXpressoIDE ? Because I didn't manage to find it. 

Basically, for me it works between around 1-256 values with a base of 16. 

I link to you a screen of my signal. That's the best number of values I can get without any troubles...

0 项奖励
回复
19,890 次查看
ErichStyger
Specialist I

I have started implementing it based on the information in the reference manual (you mentioned above) and looking at the data in the file.

0 项奖励
回复
19,869 次查看
ErichStyger
Specialist I

Hi @Skyrise ,

just in case, I have published my work-in-progress on GitHub here:

https://github.com/ErichStyger/mcuoneclipse/tree/master/MCU-Link/EnergyMeasurement

 

Erich

标记 (1)
0 项奖励
回复
19,820 次查看
Skyrise
Contributor II

Hi, @ErichStyger ,

 

I appreciate it thank you.

I'll let you know if I find something interesting for the frequency of the avg measures. 

0 项奖励
回复
19,815 次查看
ErichStyger
Specialist I

Hi @Skyrise ,

Check getNofSummaryItems() in the code I have put on GitHub. This works for me.

I'm in the process of writing a blog article with details about it.

Erich

0 项奖励
回复
19,708 次查看
ErichStyger
Specialist I

Hi @Skyrise ,

I posted an article with source code here:

https://mcuoneclipse.com/2023/07/30/data-converter-for-mcuxpresso-energy-measurement-data/

I hope it is useful for you.

0 项奖励
回复
19,701 次查看
Skyrise
Contributor II

Hi, @ErichStyger 

Thank you for your work, you're awesome ! 

19,690 次查看
ErichStyger
Specialist I

Thank you! Just keep in mind: as noted in the article, the us counting has not been sorted out completely. If I count the us time, I only get up to about 60% of the total sample time. Still investigating this.

Is the source code useful for you?

0 项奖励
回复
19,686 次查看
Skyrise
Contributor II

 @ErichStyger of course it is useful for me, I didn't try it yet because I don't have access to my computer right. As soon as I can I'll try it out !

You mean you only recover 60% of the signal or it is just the timestamp which is not correct ? 

0 项奖励
回复
19,545 次查看
ErichStyger
Specialist I

Hi @Skyrise ,

please check out the latest sources on GitHub. I worked on the timestamp thing today, and have applied a fix with some other timestamp improvements. Data looks correct on my side now.

0 项奖励
回复
19,524 次查看
Skyrise
Contributor II

Hi, @ErichStyger 

I just tried your code and it works fine for me now. 

Thank you once again for your work !

19,515 次查看
ErichStyger
Specialist I

Hi @Skyrise ,

that's really good news!

I did update my article on https://mcuoneclipse.com/2023/07/30/data-converter-for-mcuxpresso-energy-measurement-data/ with the latest findings.

I hope others will benefit from this too.

0 项奖励
回复
19,678 次查看
ErichStyger
Specialist I

I'm not clear from the documentation how the time stamps are constructed. It believe the timestamp is the time needed for the 'base' number of samples, but not sure. So in essence, the time stamps are not absolute values (as I would expect them), but relative ones.

Adding up the time of the time that way I get a total data time of around 1200 ms instead of the expected 1700 ms as shown in the IDE. Maybe I'm missing something?

So how do you read or understand the timestamp data?

0 项奖励
回复