Example working project for TFT with LPC832/834

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example working project for TFT with LPC832/834

924 Views
aaronm
Contributor IV

This is not a question: I'm just contributing a working project that demonstrates an ST7735 TFT (1.4" in my case) driven by an LPC834, though I suspect an LPC832 might also drive it, if you optimize for space so the binary will fit in flash.

It uses the TFT code base developed by Michal Kozakiewicz, github.com/michal037, found here: https://github.com/michal037/driver-ST7735S 

It uses LPC834 SDK 2.16.00 (2024-07-12), which seems to work a little better than 25_06_00, but I may have caused my own problems, there.  2.16.00 at least allows you to use the Peripherals tool to configure ADC, and SPI.

Uncompress the zip file, import the contents into a new project, and off you go.  Hope this helps someone.

Labels (1)
0 Kudos
Reply
1 Reply

866 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi @aaronm 

 

Thanks for your sharing.

 

BR

Alice