Error while compiling LPCXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error while compiling LPCXpresso IDE

2,180件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andresfrid on Sat May 31 07:47:47 MST 2014
Hello, well im having an error report while building CMSIS (and any library im trying to build), and i cant find the solution for this.

ERROR MESSAGE(readed from the console):


------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

11:29:44 **** Incremental Build of configuration Debug for project CMSISv1p30_LPC17xx ****
make all
m.AllocationBase 0x0, m.BaseAddress 0x71110000, m.RegionSize 0x80000, m.State 0x10000
C:\nxp\LPCXpresso_5.2.6_2137\lpcxpresso\msys\bin\sh.exe: *** Couldn't reserve space for cygwin's heap (0x71110000 <0x2720000>) in child, Win32 error 0
make: *** [src/core_cm3.o] Error 1

11:29:44 Build Finished (took 165ms)

--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------




ラベル(1)
0 件の賞賛
返信
1 返信

2,050件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sat May 31 08:51:07 MST 2014
There is a FAQ on that.

http://www.lpcware.com/content/faq/lpcxpresso/virtual-alloc-pointer-null-error
0 件の賞賛
返信