Error 58: crt_emu_lpc18_43_nxp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error 58: crt_emu_lpc18_43_nxp

820 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nsacks on Fri Mar 22 19:55:49 MST 2013
Hello all,

Because the Example Virtual Serial Device project from NXPUSBLib contains a space in it's directory structure (specifically Example_VirtualSerialDevice/LPC43xx M4/...) I can not successfully download code through the GUI programming tool in LPCXpresso.

So, I have attempted to compile a binary file, and download to my LPCXplorer4330's M4 core. This results in the error included at the end of this post.

Do you have any suggestions as to how I can get some code downloading? I'm running Ubuntu 12.10 x32, and the LPC-Link JTAG programmer.

I have quadruple checked file permissions, and have tried multiple combinations of AXF files or BIN files.

Thank You!




$ crt_emu_lpc18_43_nxp -wire=winusb -pLPC4330 -vendor=NXP -flash-load-exec=~/Desktop/Example_VirtualSerialDevice.bin -load-base-address=0x14000000
Ni: LPCXpresso Debug Driver v4.0 (Sep 19 2012 09:15:29)
Nc: Looked for chip XML file in /usr/local/lpcxpresso_4.3.0_1025/lpcxpresso/bin/LPC4330.xml

Nc: Looked for vendor directory XML file in /usr/local/lpcxpresso_4.3.0_1025/lpcxpresso/bin/nxp_directory.xml

Nc: Found generic directory XML file in /usr/local/lpcxpresso_4.3.0_1025/lpcxpresso/bin/crt_directory.xml

Nc: Emu(0): Conn&Reset. DpID: 2BA01477. Info: LPCLINK_1_1
Nc: SWD Frequency: 3000 KHz. RTCK: False. Vector catch: False.
Nc: Packet delay: 0  Poll delay: 0.
Nc: NXP: LPC4330  Part ID: 0x00000000
Cr:v Registered license, download limit of 128K
Et:58: Cannot open binary file 'Example_VirtualSerialDevice.bin'
标签 (1)
0 项奖励
回复
0 回复数