Errata on LPC11U3x Product Data Sheet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Errata on LPC11U3x Product Data Sheet

1,058 Views
hmyoong
Contributor III

Errata on LPC11U3x Product Data Sheet (Rev 2.3 - 8 February 2017)

 

Page 54:

The original text

the voltage divider should provide a reduction of 3.6 V/5.25 V or ~0.686 V.

 

should be changed to

the voltage divider should provide a reduction of 3.6 V/5.25 V or ~0.686.

Labels (1)
0 Kudos
Reply
1 Reply

957 Views
soledad
NXP Employee
NXP Employee

Hi,

Yes, you are right, thank you for your feedback, we will check this with our documentation team.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply