Enthernet Driver in LPC18xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enthernet Driver in LPC18xx

1,822件の閲覧回数
yuanbinzhou
Contributor II

Hi all,

I am currently trying to use Ethernet driver in LPC18xx platform and would like to port Ethernet driver into a RTOS from China. However I cannot find any ethernet driver examples on LPC OPEN Library. There are some examples in lwip_freertos project related to emac. However we do not need lwip stack and drivers in lwip_freertos project cannot be easily ported to other RTOS since it has lots of API related to Freertos and lwip . Can anyone help me?

ラベル(1)
0 件の賞賛
返信
1 返信

1,635件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Yuanbin Zhou,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.
It's the LPC18xx CMSIS-Compliant Standard Peripheral Firmware Driver Library that 
includes the EMAC demo, and please refer to it for details.
LPC18xx CMSIS-Compliant Standard Peripheral Firmware Driver Library:
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------