EmWin 5.18 crash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EmWin 5.18 crash

1,592 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by luc.vercruysse on Mon Oct 06 14:43:51 MST 2014
My system crashes after QUI_init(). When I do not call the SysTick_Config function all works fine.
It seems that the interrupt jumps to a undefined location. When I do not use EmWin library, the sys_tick interrupt is handled OK.

Any idea ??

标签 (1)
0 项奖励
回复
2 回复数

1,536 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by luc.vercruysse on Tue Oct 07 08:33:46 MST 2014
No problems with 5.24. Thanks for response !
0 项奖励
回复

1,536 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Mon Oct 06 23:41:50 MST 2014
Try a later release? Nxp are shipping 5.24 now.
http://www.lpcware.com/content/project/emwin-graphics-library
0 项奖励
回复