Eeprom endurance and Writing and erase/programming process

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Eeprom endurance and Writing and erase/programming process

1,650件の閲覧回数
javiervallori
Contributor III

Hi, I have one question about the writing and erase/programming process for the LPC43xx MCUs. In the datasheet at 50.6.2.1 section, indicates the following:

- "Partial page writes are allowed, and the EEPROM will only take locations where a word has been written for the erase/program cycle."

Does this sentence means that the writing of a word, do not affect in the ENDURANCE of another word of the SAME page? In other words, the erase/programming process is done in the hole page, or just in the writing words? Thanks in advance.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,512件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Javier,

Your understanding is correct, write the word which has never write before in the same page, don't affect the endurance of another word of the same page.
Actually, the erase/programing process is done in the whole page.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信