EXTINT3 and other EXTINTs in LPC1769

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EXTINT3 and other EXTINTs in LPC1769

1,022 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by federoasio on Tue Oct 23 08:29:47 MST 2012
Hi, I'm trying to use all the external interrupts in a project in order to detect the "end of conversion" signals from some sensors I'm using.
I was trying to use EXTINT3 and I have some problems. If I only use EXTINT3 then everything works fine, but if I also use another external interrupt, e.g. EXTINT2, then I receive interrupts from EXTINT2 in the EXTINT3 handler. I know all GPIO interrupts are connected to EXTINT3, and I guess this has something to do with this problem, but I don't know how to avoid it.

I can't avoid using EXTINT3, any ideas to solve it?

Thanks in advance.
标签 (1)
0 项奖励
回复
1 回复

1,004 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by federoasio on Tue Oct 23 12:58:09 MST 2012
I'm sorry very stupid question, I was setting the registers with = ando not with | (newbie mistake), so the response was unpredictable.
0 项奖励
回复