EEPROM with LPC4357: 180 MHz or 204 MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EEPROM with LPC4357: 180 MHz or 204 MHz

1,127件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Wed Jan 07 03:23:23 MST 2015
Does someone know details about the maximum clock of EEPROM?

According to LPC4357 user manual UM10503.pdf (version 1.8 from 28. January 2014, table 1153)
"EEPROM BASE_M4_CLK CLK_M4_EEPROM up to 204 MHz"

According to errata sheet ES_LPC435X_3X_2X_1X_FLASH.pdf (Rev. 5 — 15 August 2014):
"
Chapter 3.2 EEPROM.2
A 16 kB EEPROM is available on these parts which operates up to 180 MHz.
"

What is correct? Must CLK_M4_EEPROM be limited to 180 MHz or can it be driven with 204 MHz?

Or is it due to changes in register RWSTATE and WSTATE, so it can be used with 204 MHz instead of 180 MHz?


ラベル(1)
0 件の賞賛
返信
1 返信

1,028件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Jan 08 19:58:50 MST 2015
Hi,

The maximum clock of EEPROM is  204 Mhz as mentioned in the UM.
Thanks for pointing out the mistake in Errata sheet. It will updated in the next revision.

Thanks,
NXP Technical Support
0 件の賞賛
返信