Does the LPC-Link2 support LPC11A04 and LPC11A02?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does the LPC-Link2 support LPC11A04 and LPC11A02?

2,150 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alainbs on Mon Feb 17 07:14:02 MST 2014

Hi,

Could someone please tell me if the LPC-Link2 supports the LPC11A04 and LPC11A02?

I am asking this because according to the NXP website the LPC-Link doesn't. It appears that the LPC-Link does support LPC11A14 but not the 04 and 02.

http://www.nxp.com/knowledge-base/50809/1111414

Why does LPC-Link not work with the LPC11A02 and LPC11A04?
The LPC-Link communicates with LPC11A02/04 through the SWD pins.  The SWD pins on the LPC11A02/04 have glitch filters enabled by default.  The LPC-Link operate at a speed which gets filtered out by the glitch filter.  To use LPCXpresso with the LPC11A02/04, please use the Red Probe debugger which allows changing of the SWD clock frequency.

Kind Regards!
Alain
标签 (1)
0 项奖励
回复
6 回复数

2,123 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alainbs on Tue Mar 04 02:38:42 MST 2014
Hi,


I followed your instructions and everything is looking good, i was able to debug and program the LPC11A04 with the LPC-Link2  :D.

Thanks a lot!!

Alain
0 项奖励
回复

2,123 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Feb 28 12:11:46 MST 2014

Alain,

Extract the attached executable into the lpcxpresso/bin directory of your installation. This exec is used for the LPC-Link2 debug probe which I understand has been supplied to you.

Regards,

LPCXpresso-Support
0 项奖励
回复

2,123 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alainbs on Fri Feb 28 03:16:14 MST 2014
Hi,


i have installed LPCXpresso 7.0.0.


Best regards,

Alain
0 项奖励
回复

2,123 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 25 21:31:27 MST 2014

NXP has tested an LPCXpresso 7.0.0 patch which will allow LPC11A0x debug using the LPC-Link2.  You’ll need to first update to the latest LPCXpresso 7.0.0 release. Let us know once you've done this, and we'll either post or e-mail the patch file(s).

Regards,

LPCXpresso-Support

0 项奖励
回复

2,123 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 25 14:11:24 MST 2014
This is not correct. The LPC-Link2 should support these parts, but we have not had an opportunity to test. In principle, you will just need to reduce the Wire speed.

However, LPC-Link1 (the original) cannot support LPC11A02/4
0 项奖励
回复

2,123 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Tue Feb 25 13:34:34 MST 2014
Hi Alain,

No . LPCLink 2 does not support LPC11A04 and LPC11A02.

Thanks,

NXP Technical Support
0 项奖励
回复