Does LPC5516 support EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does LPC5516 support EEPROM

ソリューションへジャンプ
1,861件の閲覧回数
yangao
Contributor III

Hi,

As in Subject - does LPC5516 support EEPROM? Or there is a SW emulated way to store data to persist power cycle?

Regards,

Winston

ラベル(1)
0 件の賞賛
返信
1 解決策
1,845件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI yangao,

LPC5516 doesn't upport EEPROM.

If we need to program on chip Flash in run time, I would recommend referring flashiap demo code under SDK install folder. The IAP Flash project is a simple demonstration program of the SDK IAP driver. It erases and programs a portion of on-chip flash memory. A message a printed on the UART terminal as various operations on flash memory are performed.

Have a nice day,

Jun Zhang

元の投稿で解決策を見る

1 返信
1,846件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI yangao,

LPC5516 doesn't upport EEPROM.

If we need to program on chip Flash in run time, I would recommend referring flashiap demo code under SDK install folder. The IAP Flash project is a simple demonstration program of the SDK IAP driver. It erases and programs a portion of on-chip flash memory. A message a printed on the UART terminal as various operations on flash memory are performed.

Have a nice day,

Jun Zhang