Do any one has J1939 stack to work on CAN2.0 Module. Kindly help. I am working on LPC11c24 series controller to capture sensor data and broadcast it on CAN bus using J1939 protocol. I am ne to this protocol. Pl help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do any one has J1939 stack to work on CAN2.0 Module. Kindly help. I am working on LPC11c24 series controller to capture sensor data and broadcast it on CAN bus using J1939 protocol. I am ne to this protocol. Pl help

2,798 Views
sridharan
Contributor II

I am working on LPC11C24 micro controller, I need to broadcast few sensor data on CAN bus using J1939 protocol. I need to know if NXP has J1939 stack drivers. 

Some of the activity J1939 need to carry out are mentioned below:

Dynamic Address Claim support⁽¹⁾

Source Address change :PGN 0xFED8

Software version  :PGN 0xFEDA

Hardware version :PGN 0xFEEB

Broadcast Status Message :PGN 0xFFXX

Changing Status PGN values

SPN ⁽¹⁾

Configurable Massage Rate

Checksum calculation

Testing

Tags (1)
0 Kudos
Reply
2 Replies

2,428 Views
我爱下载
Contributor III

你可以参考一下以前飞思卡尔微控制的J1939的firmware,它里面有J1939的解析步骤。

0 Kudos
Reply

2,428 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi sirdharan TechM,

  Unfortunately, we still don't have the J1939 stack for LPC11C24, please refer to my reply in this post:

Please help in configuring CAN for the LPC11C24 controller 


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply