Debugging in MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging in MCUXpresso IDE

6,693 Views
DHARSAN
Contributor III

Hi 

   I'm currently working UART communication of receiving while debugging in the controller with the board, it occurs Hardfault error so that I couldn't debug. Though when working in EVK board debugging works without any issue. And I have attached the screenshot below.

0 Kudos
Reply
7 Replies

6,679 Views
_Leo_
NXP TechSupport
NXP TechSupport

Could you please tell us which MCU/part are you using please?

0 Kudos
Reply

6,653 Views
DHARSAN
Contributor III

MCUXpresso IDE V 11.8.0_1165 & LPC55S16 microcontroller

 

0 Kudos
Reply

6,642 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN

Do you mean the same example works well on EVK board, while there is issue with your own board?

How about debug a simple led or hello world demo on your custom board? Or create a new project based on your chip to test. Pay attention choose correct part number.

 

BR

Alice

0 Kudos
Reply

6,635 Views
DHARSAN
Contributor III

receiving same data in controller when transmitting different data from uart module

0 Kudos
Reply

6,625 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN 

"receiving same data in controller when transmitting different data from uart module"

->> If so, you need check your code.

 

BR

Alice

0 Kudos
Reply

6,616 Views
DHARSAN
Contributor III

But I'm working in the SDK example code  which is modified for receiving only

0 Kudos
Reply

6,491 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN 

1> So recommend you first use SDK demo without any modification.

2> Check whether enable UART clock and pin clock you used.

 

BR

Alice

0 Kudos
Reply