Debugging in MCUXpresso IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugging in MCUXpresso IDE

4,734 次查看
DHARSAN
Contributor III

Hi 

   I'm currently working UART communication of receiving while debugging in the controller with the board, it occurs Hardfault error so that I couldn't debug. Though when working in EVK board debugging works without any issue. And I have attached the screenshot below.

0 项奖励
回复
7 回复数

4,720 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Could you please tell us which MCU/part are you using please?

0 项奖励
回复

4,694 次查看
DHARSAN
Contributor III

MCUXpresso IDE V 11.8.0_1165 & LPC55S16 microcontroller

 

0 项奖励
回复

4,683 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN

Do you mean the same example works well on EVK board, while there is issue with your own board?

How about debug a simple led or hello world demo on your custom board? Or create a new project based on your chip to test. Pay attention choose correct part number.

 

BR

Alice

0 项奖励
回复

4,676 次查看
DHARSAN
Contributor III

receiving same data in controller when transmitting different data from uart module

0 项奖励
回复

4,666 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN 

"receiving same data in controller when transmitting different data from uart module"

->> If so, you need check your code.

 

BR

Alice

0 项奖励
回复

4,657 次查看
DHARSAN
Contributor III

But I'm working in the SDK example code  which is modified for receiving only

0 项奖励
回复

4,532 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN 

1> So recommend you first use SDK demo without any modification.

2> Check whether enable UART clock and pin clock you used.

 

BR

Alice

0 项奖励
回复