Debugging in MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging in MCUXpresso IDE

7,006件の閲覧回数
DHARSAN
Contributor III

Hi 

   I'm currently working UART communication of receiving while debugging in the controller with the board, it occurs Hardfault error so that I couldn't debug. Though when working in EVK board debugging works without any issue. And I have attached the screenshot below.

0 件の賞賛
返信
7 返答(返信)

6,992件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Could you please tell us which MCU/part are you using please?

0 件の賞賛
返信

6,966件の閲覧回数
DHARSAN
Contributor III

MCUXpresso IDE V 11.8.0_1165 & LPC55S16 microcontroller

 

0 件の賞賛
返信

6,955件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN

Do you mean the same example works well on EVK board, while there is issue with your own board?

How about debug a simple led or hello world demo on your custom board? Or create a new project based on your chip to test. Pay attention choose correct part number.

 

BR

Alice

0 件の賞賛
返信

6,948件の閲覧回数
DHARSAN
Contributor III

receiving same data in controller when transmitting different data from uart module

0 件の賞賛
返信

6,938件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN 

"receiving same data in controller when transmitting different data from uart module"

->> If so, you need check your code.

 

BR

Alice

0 件の賞賛
返信

6,929件の閲覧回数
DHARSAN
Contributor III

But I'm working in the SDK example code  which is modified for receiving only

0 件の賞賛
返信

6,804件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN 

1> So recommend you first use SDK demo without any modification.

2> Check whether enable UART clock and pin clock you used.

 

BR

Alice

0 件の賞賛
返信