'Debug port fail' while accessing T1022 using Lauterbach Trace32

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

'Debug port fail' while accessing T1022 using Lauterbach Trace32

3,189 次查看
vgupta1
Contributor I

Hi, I am using T1022 in my design and I am trying to access processor via Lauterbach tool Trace32 power view. But I am encountering the error: 'debug port fail' or 'CPU setting: 2 cores, detected: 1 core. Check your CPU settings '. The tool is able to read SVR and PVR and also reading the correct processor using diag command. Also, the processor is successfully coming out of reset by driving HRESET high and ASLEEP high to low, hence indicate that PLLs are also locking. We have set hardcoded RCW to 0x9E configuration. Attached is the Trace32 message dump.

Please suggest what may be the issue.lauterbacht1022

标记 (2)
0 项奖励
回复
2 回复数

2,999 次查看
ufedor
NXP Employee
NXP Employee

Please report the issue to the Lauterbach technical support first.

In case of further questions please provide their response in th Qor IQ space.

0 项奖励
回复

2,999 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Please post this question in the QorIQ space ... this is the LPC community.

0 项奖励
回复