Debug LPC1549 using IAR IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug LPC1549 using IAR IDE

1,593件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by afiqahlaa on Mon Aug 03 20:46:35 MST 2015
Good morning and hye!

I am wondering, do I need any Debugger Probe for be to debug code using IAR IDE for board LPC1549?
FYI, I am using LPC1549 together with rev. B board which is demo board of OM13067.
http://www.nxp.com/demoboard/OM13067.html

Thank you in advance!
ラベル(1)
0 件の賞賛
返信
1 返信

1,566件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Aug 04 00:32:02 MST 2015
Soft booting of the debug probe is only supported using LPCXpresso IDE. For use with IAR, you'll need to program CMSIS-DAP or J-Link firmware into the on board debug probe's flash, which can be done using LPCScrypt. For information on this see:

https://www.lpcware.com/LPCXpressoV2Boards

https://www.lpcware.com/LPCScrypt

Regards,
LPCXpresso Support


0 件の賞賛
返信