DMA with AES

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMA with AES

4,482件の閲覧回数
Jgeorge
Contributor I

Hi,

I am trying to Run AES using DMA.

I  tried for last three days, but could not proceed further.

How I did?

1.I too sample code of DMA Memory to Memory from SDK

2.Added the AES header and Driver file in it.

3.Changed the AES configuration accordingly w.r.t DMA.

4.Then compiled and execute but code is stuck in while loop.

Please can anyone tell is this correct way of doing?

I read there are some trigger and input source for DMA request but couldn't find any example how to do it.

Can anyone share the pseudo code?

 

 

ラベル(1)
0 件の賞賛
返信
9 返答(返信)

4,474件の閲覧回数
Jgeorge
Contributor I

No I haven't used trigger source but yes I read about it in UM ,can you please tell me any reference in demo code for trigger source or do I have to create my own.

yes I am using AES module of LPC55s69.I am using software key for AES.

0 件の賞賛
返信

4,433件の閲覧回数
Jgeorge
Contributor I

Hi Alice_Yang,

Sure,Please see the code i have done.You can also run the code at your side.Waiting for your reply.

0 件の賞賛
返信

4,429件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jgeorge,

So what's your problem now? I think you can debug with breakpoint or step by step first confirm the detail

issue.

 

BR

Alice

0 件の賞賛
返信

4,426件の閲覧回数
Jgeorge
Contributor I

Hi Alice_Yang,

Thanks for your code suggestion.

The code which i shared is not complete.

I have completed the code now and could debug with breakpoint step by step also.

The DMA transfer is  working fine but the encrypted data from the output/DIGEST register is coming incorrect.

I am having doubt in giving the user key that is  userkey should be loaded after the DMA transfer or before transfer?

I am doing before DMA transfer.

please suggest if there is any other way for getting output/DIGEST register.

Note:I am just a beginner !

0 件の賞賛
返信

4,407件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jgeorge,

Yes, giving user key before DMA transfer is no problem.

It seems your code disable the use key and other AES encrypt related code.

Recommend first development base on hashcypt demo under SDK, change it to your request, and confirm the AES work well , the DIGEST data is right.  then add DMA request on it.

 

BR

Alice

0 件の賞賛
返信

4,402件の閲覧回数
Jgeorge
Contributor I

Hi Alice_Yang

 

Sure.Thanks for your suggestion

Regards,

Jacob

0 件の賞賛
返信

4,461件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jgeorge,

Please refer to "Configure the DMA as follows: ..." in UM to config DMA, 

and the SDK demo with DAM, for example "usart_dma_transfer".

 

BR

Alice

0 件の賞賛
返信

4,455件の閲覧回数
Jgeorge
Contributor I

Hi Alice_Yang,

Yes thanks for the information.

I have started exploring UART DMA code ,it's understandable now.

According to that only I am configuring for AES.

Sure I will share my complete code once I configure all the registers by tomorrow EOD.

Please see to it and looking forward for your feedback

0 件の賞賛
返信

4,477件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jgeorge,

Could you please show more information about your application.

The trigger Source of DMA ?

And do you use AES module of LPC55 or just software AES?

 

BR

Alice