DHT11 Test aplication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DHT11 Test aplication

2,325件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Raigetix on Thu May 12 19:30:36 MST 2016
Hi.

I was looking for an aplication to read a DHT11 for lpc, beacuse I need it for a project to my university, but I didn't find any library for that. So I made one and I want to give that to any one that need.

I test this with the DHT11 to 3,3v and with a 5k pull-up resistor. The data cable of the sensor is conected to the P1.18 (CAP1.0).
The code is commented in spanish but is not to hard to understand without reading the coments.

So I hope have helped even a little.

Original Attachment has been moved to: DHT11_main.zip

ラベル(1)
0 件の賞賛
返信
1 返信

1,850件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信