DAC and DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DAC and DMA

1,101件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by FrankAndersen on Wed Jul 17 04:39:14 MST 2013
Hi,

MCU is LPC1788.

I am using the DAC together with DMA ch1 to play sounds, must of the time, it works, but sometimes it stops working, the error is hard to reproduce, and I have not yet been able to reproduce very often.

The DMA transfer does not end, and when the error happens, even thoug I init the DMA channel again, it does not start.

The source for the DMA is external flash.

Any one out there using the DAC together with the DMA?

Best regards,

Frank Andersen
ラベル(1)
0 件の賞賛
返信
0 返答(返信)