DAC Problem on LPC-Link 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DAC Problem on LPC-Link 2

2,025 Views
nicokiz
Contributor I

Hello everybody,

I've got a question regarding the LPC-Link 2-Board.

Can somebody give me an example, how to use the Digital-to-Analog-Converter (DAC)? I found this example: http://docs.lpcware.com/lpcopen/v1.03/group___e_x_a_m_p_l_e_s___p_e_r_i_p_h__18_x_x43_x_x___d_a_c.ht... , but it does not work. There are 2 problems:

First: Pin 4_4 does not exist on the LPC Link 2 Board.

Second: How do I use the UART? ("Use UART to monitor this demo.")

Best Regards!

Nico

0 Kudos
Reply
2 Replies

1,674 Views
soledad
NXP Employee
NXP Employee

Hi,

You can download the LPCOpen for LPC-Link2 from the following link:

LPCOpen Software for LPC43XX|NXP 

After download it, you will find uart and dac example codes.

I hope thi helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,674 Views
nicokiz
Contributor I

Hello soledad,

no, did not work at all. I'm sorry, but these example codes are just disgusting.

Hope this helps.

Have a nice day,

KIZ

0 Kudos
Reply