Custom board bringup for LPC4333

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom board bringup for LPC4333

2,305件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sanjeevudupi on Tue Mar 12 22:54:27 MST 2013
Hi all,
We have a custom board which have LPC4333 as the main processor.Can any body guide me , how to start with the board ?
I have few queries.
1.Whether boot code is required to start the board ?
2.Whether boot code is already there in the on-chip ROM of the LPC4333 ?
3.If boot code is not there then where I will get the boot code and how I will program the board with boot code?
4.Is there any other procedure to bring up the board ?

Please help on these issues .Thanks in Advance.
sanjeevudupi
ラベル(1)
0 件の賞賛
返信
1 返信

2,186件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alex on Wed Mar 13 01:51:12 MST 2013
Hi,

the processor already has boot code inside its internal ROM.

You should take a look to the user guide for more information about how it works.

http://www.nxp.com/documents/user_manual/UM10503.pdf

The boot ROM and the available boot modes are explained in chapter 5.

Regards,
Alex
0 件の賞賛
返信