Currently using LPC82x, but need to also use Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Currently using LPC82x, but need to also use Linux

1,254件の閲覧回数
jeremyprice
Contributor I

Apologies, as I am not technical.

We have some code running on the LPC82X. However we now need to run a Linux processor. Is there a product we can use where we can port the existing code onto the upgraded processor.

Any help greatly appreciated.

Jeremy

0 件の賞賛
返信
1 返信

1,193件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please continue the follow up in this thread: Advice on upgrade from LPC82x to Linux based processor 


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信