Could not connect to core. No connection to chip's debug port in LPC55s36

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could not connect to core. No connection to chip's debug port in LPC55s36

886 Views
Shravan_Vailaya
Contributor I

Hello, 

I am currently working on LPC55s36-EVK board (https://www.nxp.com/part/LPC5536-EVK#/ )and it was working properly for last 6 months. But while debugging a project the no connection to the chips debug port error appeared as shown in the figures attached below. 

I tried to connect the board with other PC and it works correctly and also I have another LPC55s36-EVK board and it works with my PC.

I have deleted the .launch file and tried to rebuild again but it didn't work. I changed my workspace and reinstalled my IDE also that also didn't help. I have also updated the driver in my device manager which also didn't work. 

 

1.png2.png3.png

Thanks and Regards

Shravan

 

0 Kudos
Reply
1 Reply

855 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Shravan_Vailaya 

1. You can erase the flash in IAR mode.

you need to short the jumper J43 3-4.

HangZhang_0-1721297364999.png

And then erase the flash.

HangZhang_1-1721297499032.png

2. Cancel the J43 jumper and program the code.

Hope this will help you.

BR

Hang

0 Kudos
Reply