Confusing for Peripherials config for LPC55S16 in sample code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Confusing for Peripherials config for LPC55S16 in sample code

1,125 Views
ygao
Contributor I

Hi,

For a I2C setting to use Flexcomm4, it needs to config clock on Clocks config for FXCOMCLK4, and config Flexcomm4 pins to be I2C in Peripherials config, right?

However, in LPC55S16 sample code, e.g., lpcxpresso55s16_multi_peripherals_test, non clock is configured in Clocks config for Flexcomm4, and non I2C is configured in Peripherals config. Why?

Is it because all the code are input manually instead of generating by configs?

Thanks,

Winston

Labels (1)
0 Kudos
Reply
1 Reply

1,112 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ygao 

Yes, some of examples not use Configure tool to config. The code is  input manually .

 

BR

Alice

0 Kudos
Reply