Communication with SD Card through SSP perippheral fails with ROR error.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Communication with SD Card through SSP perippheral fails with ROR error.

942件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ramana on Wed Jun 01 23:09:17 MST 2016
hi

I am using SSP peripheral in SPI mode to communicate with the SD Card and DMA to transfer the data to the SSP peripheral. here I am getting ROR error frequently in SSP peripheral. Temporary solution to the problem I have made is resetting the DMA and SSP peripheral but it disturbs the other DMA transfers. but it is not a good one to reset the SSP and DMA. anybody please help me in getting out of this issue.

Thanks n regards
Shankar
ラベル(1)
0 件の賞賛
返信
1 返信

900件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信