Chip power consumption when both Cores sleeping.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Chip power consumption when both Cores sleeping.

1,374 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andypevy on Wed Jan 28 09:06:36 MST 2015
Hi,

     Is there a specified figure (Or even a typical one) for the chip
power consumption when both cores are sleeping. The spec has
M0 running and M4 sleeping and the other way around, but not both
asleep.

Thanks,
Andy Pevy
Labels (1)
0 Kudos
Reply
1 Reply

1,356 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Wed Jan 28 09:24:00 MST 2015
Hi andypevy,

When both cores are in sleep mode, the MCU is in our "Sleep mode" state. You can expect the MCU to draw about 1.21 mA. For more information in regards to the low power modes, check out our low power application note:

http://www.lpcware.com/content/nxpfile/lpc54100-low-power-modes-and-wake-times-application-note
0 Kudos
Reply