Can't connect lpclink2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't connect lpclink2

1,694 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jerrylwb on Fri Aug 01 00:26:12 MST 2014
Hi,

    I am tring the lpcexpresso board 1549 and I had compile and run the "blinky" sample successfully with Ebed yesterday. Today  I want to configurate the plclink2 use DFU programmer(LPC_Link2_Config_tool_v1_11_1) as jlink, due to use the IAR IDE .
    But It's a pity that the programming field! And even I can't connect the lpclink2 , the programme software can't find usb(see attached image). I thought that the LPC4322 need to programmed again ,how to programme it?  where is the bin file?
Labels (1)
0 Kudos
Reply
2 Replies

1,661 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jerrylwb on Fri Aug 01 20:02:38 MST 2014
   I get it ,Thank you very mcuh! :)
0 Kudos
Reply

1,661 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Fri Aug 01 00:50:04 MST 2014
To restore LPC-Link2 functionality, JP2 must be inserted. LPCXpresso will automatically detect and download the correct image.
For more information, see:
http://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link2
0 Kudos
Reply