Can PC communicate with USB HID with INT EndPoint?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can PC communicate with USB HID with INT EndPoint?

1,183件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by iamonline on Sat Aug 09 22:23:58 MST 2014
Hi:
    There are 4-cdc & 1-hid device(composite device) on my LPC1768 Platform. When power on, usb enum is OK. I can also write data to the CDC Endpoint by calling USB_WriteEP() function and PC can receive the data. But when I write data to the HID IN EndPoint, PC can not read these data. Can any body give me some advice why I cannot write data to HID EP directly? Can only the HID exchange data with PC by HID report?
    Thanks a lot.
ラベル(1)
  • USB

0 件の賞賛
返信
0 返答(返信)