CMSIS-DAP rev D2 (C) 2017

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CMSIS-DAP rev D2 (C) 2017

1,658 次查看
prashantmadalag
Contributor I

Hello Everyone,

I am using the CMSIS-DAP rev D2 (C) 2017 board to dump the code for my external LPC MCU 1769 but I am getting error message like - " No compatible emulators available.
They may be disconnected, not powered, already in use or not compatible with this target"  while trying to dump the code with tool "LPCXpresso v8.2.2 [Build 650] [2016-09-09] "

Please help out me.

标记 (1)
0 项奖励
回复
2 回复数

1,490 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

I'm not sure what you mean by a "CMSIS-DAP rev D2 (C) 2017", but it is possible that you are using a debug probe introduced after the last version of LPCXpresso IDE was released and that LPCXpresso IDE doens't know about. In which case you could try using the MCUXpresso IDE product instead (which has superseded the old LPCXpresso IDE). 

Regards,

MCUXpresso IDE Support

0 项奖励
回复

1,490 次查看
prashantmadalag
Contributor I

Hi Support Team,

Yes , I was using that debugging probe. And for that their binary file was not supported (older or something). 

I changed the binary file and that's worked.

Thank you. 

0 项奖励
回复