CAN based project using lpc1769 and LPCOpen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN based project using lpc1769 and LPCOpen

1,467 Views
aniketsgajare
Contributor I

I am trying to implement a simple project where I send a message from node 1 to node 2 using CAN. Both the nodes are lpc1769 boards. I suppose there are some issues with the code. As I am a beginner, I request you to provide any reference codes I can look into(polling implementation will be more helpful).

Thanking you in advance.

Labels (3)
0 Kudos
Reply
1 Reply

1,398 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Aniket Gajare,

I recommend you refer to the "periph_can" demo under LPCOpen, there is a readme.txt ,

introduce how to use and config board in detail, please download it at :

LPCOpen Software for LPC17XX|NXP 

pastedImage_3.png

pastedImage_2.png

If have any question when using , please contact us without any hesitate.

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply