Bug in swm_8xx.h for LPC82x chips

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug in swm_8xx.h for LPC82x chips

1,010 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by john78727 on Fri Jan 02 10:43:47 MST 2015
void Chip_SWM_FixedPinEnable(CHIP_SWM_PIN_FIXED_T pin, bool enable);

/**
* @briefEnables a Fixed Function Pin in the Switch Matrix
* @parampin: Pin to be enabled
* @returnNothing
*/
STATIC INLINE void Chip_SWM_EnableFixedPin(CHIP_SWM_PIN_FIXED_T pin)
{
LPC_SWM->PINENABLE0 &= ~((1 << (uint32_t) pin) | SWM_PINENABLE0_RESERVED);
}

I was enabling I2C0 in the fixed pin register using this call. When I did so it also enabled all the ADC pins because the SWM_PINENABLE0_RESERVED definition was not correct for the LPC824 chip. I hope someone will fix it here:

/**
* @brief LPC8XX Switch Matrix register block structure
*/
typedef struct {
#if defined(CHIP_LPC82X)
__IO uint32_t PINASSIGN[12];/*!< Pin Assign register array */
__I  uint32_t RESERVED0[100];
#else
__IO uint32_t PINASSIGN[9];/*!< Pin Assign register array */
__I  uint32_t RESERVED0[103];
#endif
__IO uint32_t PINENABLE0;/*!< Pin Enable register */
} LPC_SWM_T;

#define SWM_PINENABLE0_RESERVED  (~0x1ff)
/**

The define should be (~0x1ffffff) for the LPC82x chip :-)

Have A Nice Day,

Regards,
John

Labels (1)
0 Kudos
Reply
1 Reply

966 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Sat Jan 03 18:10:55 MST 2015
Yes, already reported.  http://www.lpcware.com/content/forum/lpc82xbuf-lpcopen-swm-driver
0 Kudos
Reply