Binary which can run at different address locations

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Binary which can run at different address locations

1,007件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by veejaykarthik on Fri Mar 11 04:41:00 MST 2016
Hi Members,

We are using LPC2148 and we would like to know the following.

How to build a single binary file which can run from different locations Eg: 0x4000 and 0x10000

The binary file will be transferred to LPC2148 over usb and copied to different locations in Flash. Using bootloader, the binary can be invoked.

Is it possible to create a single binary which can run from different address locations?

Eg: Using position independent options like --rwpi. --ropi.


ラベル(1)
0 件の賞賛
返信
1 返信

960件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信