Beginner's question on using LPC812-MAX board with LPCXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Beginner's question on using LPC812-MAX board with LPCXpresso

1,255件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vadiode on Sun May 31 22:41:27 MST 2015
I am using LPCXpresso 7.7.2, and trying to run the example program "periph_blinky" in LPCOpen package. It compiles fine. If I connect the LPC812-MAX board to my PC (Windows 7 x64) with the USB cable directly, PC cannot connect to Redlink server. And then I try LPCLink 2 board (connecting the JTAG on two boards together, using J7 on LPCLink 2). On starting the debugging session, it gives error like this :

Error in final launch sequence
Error: Error reported by server (redlinkserv.exe):
RedlinkAPI: Wire Ack Fault - target connected?
Redlink Server has been terminated and will be restarted.
Please restart your debug session.
If the problem recurs, please power cycle your debug probe and restart LPCXpresso.
Error: Error reported by server (redlinkserv.exe):
RedlinkAPI: Wire Ack Fault - target connected?
Redlink Server has been terminated and will be restarted.
Please restart your debug session.
If the problem recurs, please power cycle your debug probe and restart LPCXpresso.

Could anyone please advise?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,181件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vadiode on Mon Jun 01 20:14:19 MST 2015
Thanks. Shorting JP1 on LPC812-MAX works.
0 件の賞賛
返信

1,181件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun May 31 23:59:28 MST 2015
The normal reason for failing to debug using the built in probe on these boards is that you have not installed the required mbed Windows serial driver.

And if you want to use an external debug probe such as LPC-Link2 with the board, then please ensure that you have fitted a jumper on JP1 (to disable the onboard debug).

For more information, please see:

http://www.lpcware.com/content/devboard/lpcxpresso-max-developer-boards

Regards,
LPCXpresso Support
0 件の賞賛
返信