BUTTON_SetReactOnLevel()

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BUTTON_SetReactOnLevel()

2,375件の閲覧回数
wangkuan1213
Contributor I

The emwin version I used is 5.30,my cpu is lpc1788.When I used BUTTON_SetReactOnLevel() function ,it didn't work! I also  configuration option BUTTON_REACT_ON_LEVEL 1.

Can you help me?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,207件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

Unfortunately, the support for the emwin API is not supported by NXP, you can contact directly to SEGGER.

emWin related - SEGGER - Forum 

 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,207件の閲覧回数
wangkuan1213
Contributor I

I download this emwin5.30 on NXP support,and I understand from SEGGER that this emwin5.30 is changed by NXP .

0 件の賞賛
返信