/* Definitions for error constants. */ #define ERR_OK 0 /* No error, everything OK. */ #define ERR_MEM -1 /* Out of memory error. */ #define ERR_BUF -2 /* Buffer error. */ #define ERR_TIMEOUT -3 /* Timeout. */ #define ERR_RTE -4 /* Routing problem. */ #define ERR_INPROGRESS -5 /* Operation in progress */ #define ERR_VAL -6 /* Illegal value. */ #define ERR_WOULDBLOCK -7 /* Operation would block. */ #define ERR_USE -8 /* Address in use. */ #define ERR_ISCONN -9 /* Already connected. */ #define ERR_IS_FATAL(e) ((e) < ERR_ISCONN) #define ERR_ABRT -10 /* Connection aborted. */ #define ERR_RST -11 /* Connection reset. */ #define ERR_CLSD -12 /* Connection closed. */ #define ERR_CONN -13 /* Not connected. */ #define ERR_ARG -14 /* Illegal argument. */ #define ERR_IF -15 /* Low-level netif error */  | 
 
/* Low level init of the MAC and PHY */
static err_t low_level_init(struct netif *netif)
{
struct lpc_enetdata *lpc_netifdata = netif->state;
/* Initialize via Chip ENET function */
Chip_ENET_Init(LPC_ETHERNET, BOARD_ENET_PHY_ADDR);
/* Save MAC address */
Chip_ENET_SetADDR(LPC_ETHERNET, netif->hwaddr);
/* Initial MAC configuration for checksum offload, full duplex,
   100Mbps, disable receive own in half duplex, inter-frame gap
   of 64-bits */
LPC_ETHERNET->MAC_CONFIG = MAC_CFG_BL(0) | MAC_CFG_IPC | MAC_CFG_DM |
   MAC_CFG_DO | MAC_CFG_FES | MAC_CFG_PS | MAC_CFG_IFG(3);
/* Setup filter */
#if IP_SOF_BROADCAST_RECV
LPC_ETHERNET->MAC_FRAME_FILTER = MAC_FF_PR | MAC_FF_RA;
#else
LPC_ETHERNET->MAC_FRAME_FILTER = 0;/* Only matching MAC address */
#endif
/* Initialize the PHY */
#if defined(USE_RMII)
if (lpc_phy_init(true, msDelay) != SUCCESS) {
return ERROR;                 <-----------------------------------!!!!!!!!!!!!!!!! - Incorrect - !!!!!!!!!!!!!!!!!!!!!!!!
}
intMask = RDES_CE | RDES_DE | RDES_RE | RDES_RWT | RDES_LC | RDES_OE |
  RDES_SAF | RDES_AFM;
#else
if (lpc_phy_init(false, msDelay) != SUCCESS) {
return ERROR;                 <-----------------------------------!!!!!!!!!!!!!!!! - Incorrect - !!!!!!!!!!!!!!!!!!!!!!!!
}
intMask = RDES_CE | RDES_RE | RDES_RWT | RDES_LC | RDES_OE | RDES_SAF |
  RDES_AFM;
#endif
/* Setup transmit and receive descriptors */
if (lpc_tx_setup(lpc_netifdata) != ERR_OK) {
return ERR_BUF;
}
if (lpc_rx_setup(lpc_netifdata) != ERR_OK) {
return ERR_BUF;
}
  |