Audio mixer project AN14531SW import issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Audio mixer project AN14531SW import issue.

Jump to solution
1,455 Views
delphin
Contributor I

I tried importing the AN14531SW project file for the application note AN14531, but MCUExpresso IDE does not recognize it as a project, so the import function is not working.

Labels (4)
0 Kudos
Reply
1 Solution
1,436 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @delphin 

The AN14531SW project is not a MCUXpresso project, it is the IAR project.

Harry_Zhang_0-1742292879137.png

Please open it with IAR IDE.

BR

Harry

View solution in original post

2 Replies
1,437 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @delphin 

The AN14531SW project is not a MCUXpresso project, it is the IAR project.

Harry_Zhang_0-1742292879137.png

Please open it with IAR IDE.

BR

Harry

1,431 Views
delphin
Contributor I

Thanks..

0 Kudos
Reply