Audio Class code generation not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Audio Class code generation not working

2,608件の閲覧回数
asca
Contributor I

Greetings,

I'm using the MCUXpresso version 24.12 with the LPC5526 SDK version for USB stack 2.11.0.

When I try to configure the USBHSD interface for Audio control and streaming, I get the following error: "Issue: "USB device audio" driver is missing in the project." However this component IS included in the SDK and enabled in the SDK manager. The peripheral is also enabled but the code cannot be generated because of this error.

Please see the screenshots in the attachement and the .mex config file.

This happens regardles of the audio interface version (both on 1.0 and 2.0).

What could be the possible cause of this issue?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,419件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi  

I created a new LPC5526 project under IDE 24.12 and SDK 25.03. I didn't see error. How to reproduce the error?

ZhangJennie_1-1748425682934.pngZhangJennie_1-1748425682934.png

 

ZhangJennie_0-1748425430796.pngZhangJennie_0-1748425430796.png

Thanks,

Jun Zhang

0 件の賞賛
返信

2,444件の閲覧回数
domtom555
Contributor I

Hi,

I have the same problem, did you solve it by any chance?

BR

0 件の賞賛
返信