Are there any USB HID example for LPC1768?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are there any USB HID example for LPC1768?

1,718件の閲覧回数
yan_m
Contributor I

I just found this: LPCOpen Software for LPC17XX | NXP

But these examples are for LPC1788 and LPC1769.

Does anyone know where I can find an example?

タグ(2)
0 件の賞賛
返信
1 返信

1,673件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

There is no example for LPC1768, please use LPCopen for LPC1769 for your device instead.

The only difference between LPC1768 and 1769 is max CPU speed. LPC1768 is 100MHz; LPC1769 is 120MHz.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信