About the Debug Probe on LPCXpresso CD Eval. Board for LPC1769(OM13085)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the Debug Probe on LPCXpresso CD Eval. Board for LPC1769(OM13085)

1,277件の閲覧回数
doini
Contributor III

Can I use the CMSIS-DAP debug probe on LPCXpresso CD Eval. Board for LPC1769 (OM13085) to debug my own designed board with LPC1769 ?

If yes, how can I connect the CMSIS-DAP debug probe to my own designed board ?

If not, what other Eval. Board for LPC17xx exists, which can offer me the possibility to use the debug probe with other external board ?

I mention that I use the LPCXpresso IDE.

I would appreciate any answer.

Thank you,

Doini 

ラベル(3)
0 件の賞賛
返信
1 返信

1,062件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

No, the probe on the LPCXpresso1769-CD board is only intended for use debugging the onboard MCU, not an MCU mounted on a separate board.

If you want a probe to debug other boards (and also usable with the CD board), you could consider the LPC-Link2.

Regards,

LPCXpresso Support

0 件の賞賛
返信