About PRINT of .5.0_LPCXpresso54608

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About PRINT of .5.0_LPCXpresso54608

1,551 次查看
bdbz
Contributor I

Now,i'm working on lpc54608.I used the lpcxpresso54608 of SDK2.5.0_LPCXpresso54608 code(usart_polling project).i can tx and rx to the com software.but PRINT can work.do you have any sugesst?thanks !

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,486 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello 周 周,

Please pay attention to the below tips:

1) "SDK debug console" choose "UART  console":

pastedImage_1.png

2) Choose the right COM port on terminal. The PRINTF transfer through  LPC-LINK USB port(J8) on board.

3) If still can't , try the Hello_world SDK demo , just connect board with J8 port, config as 1), then run it .

Hope it helps,

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------