About ISP of LPC1768

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About ISP of LPC1768

1,888 次查看
lio0702
Contributor I

Hello,

      I'm working on a software, as Flash Magic, with LPC1768 through ISP commands. Unfortunately, it worked pretty well in the early stages until the 'G 0 T' command don't work. The 'G' command is as follows. 

pastedImage_2.png

      So, it was unlocked before runing the 'G 0 T',and return value was 0.  but the code didn't work at 0x0000000 of flash. Curiously, it worked well after reset the microcontroller by manual operation.

      Any helps/suggestions will be a great help to me.

      Looking forward to your early reply.

      Thanks.

      Yu Lio

标签 (1)
0 项奖励
回复
2 回复数

1,573 次查看
castor_xu
Contributor I

when use Go, you should bear in mind that it is still in ISP mode, not in the user code mode.

the main difference is the system clock,see your image below.

0 项奖励
回复

1,573 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Yu lio,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to the statement, I think you miss call the ISP Unlock command prior to calling the Go command. So please give a try.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复