AN11780 I2C Protocol and Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN11780 I2C Protocol and Configuration

1,639 Views
awseiger
Contributor I

Hello,

In AN11780, there is reference to "I2C-util.exe" which is used to interface with the SBL. Is the I2C protocol documented anywhere? I cannot seem to find it.

Secondly, is it possible to control other I2C parameters within the closed-source SBL, like adjusting I2C slave address or adjusting which I2C pins are utilized by the SBL?

Thanks,

Alex

Labels (1)
0 Kudos
Reply
1 Reply

1,632 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello awseiger,

Sorry it is not possible to get the source code of this application and  I2C protocol.

 

BR

Alice

0 Kudos
Reply