ADC pins permanently grounded in LPC2368

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC pins permanently grounded in LPC2368

1,193件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ramana on Thu Nov 27 23:29:53 MST 2014
       I'm using 6 ADC channels of lpc2368 to measure currents in my project. The issue is, I have been facing regular failures of ADC channels over long run. After some days at site, the ADC readings are becomes 0, when I debug the hardware, i have observed that, some of the ADC input pins of LPC2368 are showing short to Gnd of Controller.
    
      The circuit block diagram is in the attachment. It has been a big problem to me, need to replace the controller every time when the failure is observed. Please suggest me how can I prevent these failures.

Every suggestion is appreciable.

Thanks in advance


      
     
      
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,173件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ramana on Fri Nov 28 20:49:27 MST 2014
ok, Thank u.

0 件の賞賛
返信

1,173件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Nov 28 02:18:36 MST 2014
My suggestion. Don't double post!
0 件の賞賛
返信